AXIS#.VL.AINSCALE

Description

AXIS#.VL.AINSCALE is an analog velocity scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 1 (analog velocity mode).

The value entered is the motor velocity per 1 V of analog input. This value may be either higher or lower than the application velocity limit (AXIS#.VL.LIMITP orAXIS#.VL.LIMITN ), but the actual analog I/O will be limited by AXIS#.VL.LIMITP or AXIS#.VL.LIMITN .

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

Rotary: RPM"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s
See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

0 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.AINSCALE 0x5011 0x9 UDINT 1000:1 - RW False
AXIS2.VL.AINSCALE 0x5111 0x9 UDINT 1000:1 - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen